SUG_Wiser_Home_UK_IRL_WH-04

Troubleshooting

This topic explains the solutions to problems with the system, devices and configuration settings.

HUB

Symptom

Possible cause

Solution

Not able to perform offline firmware update.

The older app versions do not support offline updates.

Update the app to version 7.4.0.

Offline updates will not work on hubs running a version below 4.42.28.

Complete the commissioning process and allow the firmware to update automatically.

Offline updates will fail if the screen gets locked during the firmware updating process.

Make sure the screen remains unlocked during the updating process. You can set your phone’s Auto‑Lock to Never in your device settings.

When adding a device, the device is rejected or will not join.

The device may not be supported by the system.

Only use devices listed in List of Wiser Devices.

The device is not able to connect with the Hub/HubR. After pressing 3 times, the device LED blinks amber for 30 s.

Pairing mode has changed.

Press the Reset button on the device 3 times then hold for 20 s, until the LED blinks red. The device should reboot into the correct mode.

The hub is not communicating or receiving updates.

IPv4 is not enabled in the network settings.

Make sure that IPv4 is enabled in your local area network and Internet settings on your Internet provider’s router. Systems configured as IPv6-only will impact the hub’s ability to communicate and receive software updates.

The system cannot connect to the internet via the Wi-Fi® network router.

The router port settings may not be properly set for the system to access the internet.

Check that the following router ports are open:

Host

Protocol

Port

Description

hub.foundries.io

TCP

443

Docker container registry

hub-auth.foundries.io

TCP

443

Docker registry authentication service

storage.googleapis.com

TCP

443

OSTree and Docker redirects

api.foundries.io

TCP

443

If using lmp-device-register

app.foundries.io

TCP

443

If using lmp-device-register

cnm-ih-na.azure-devices.net

AMQP

5671

Hub to cloud connection

prd-ih-eu.azure-devices.net

AMQP

5671

Hub to cloud connection (only for Wiser HubR)

ota-lite.foundries.io

TCP

8443

Device gateway

ostree.foundries.io

TCP

8443

OSTree server for updates

If you face any issues in commissioning the device, refer to the troubleshooting section of the specific device user guide.

Refer to List of Wiser Devices for the links to Device user guide for each devices.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.