Google Home
Google Home is a brand of smart speakers that work similarly to Amazon Echo. Google’s intelligent PA, Google Assistant, is equivalent to Amazon’s Alexa. Google Home is also available on all Android devices and does not require the use of the ‘Smart Speakers’.
The user can speak a profusion of commands to request information, or ask the Google Assistant to perform an action such as play music, video playback, report news, access home automation. All of this can all be controlled from a Google Home device.
Configuring Wiser Home with Google Home
-
Tap
to find different cloud services. -
Tap on Google Assistant option. This will open the Google assistant app on your smartphone to link to Wiser system.
-
Enter the user name and password you have setup for your Wiser system and tap Done.
-
Grant the required permissions to allow you to discover all the Wiser devices you have setup, and to control your wiser system using google assistant app and by using voice command.
Changes made with Google Home
If a Device is following a Schedule, any setting changed by Google Home will last until the next event in the Schedule. If the Device is running in manual mode, any command to Google Home will remain in place until the next command or manual setting.
Common Wiser commands for Google Home
Listed below are common Wiser commands used with Google Home:
-
Inquiry: “OK Google, is the light in bedroom ON?”
-
Set Light Brightness: “OK Google, set the living room lights to 50% brightness”
-
Turn Lights On/Off: “OK Google, turn On/Off the kitchen lights”
-
Open/Close Shutters: “OK Google, close the bedroom shutters”
-
Active Away Mode: “OK Google, turn on Away Mode"
-
Activate Moments: “OK Google, turn on bedtime Moment”