SUG_Wiser_Home_Australia_WHP-04

Compatible Wiser Devices for Matter Bridge

Following are the Matter bridge compatible devices:

Refer to List of Wiser Devices for the links to Device user guide for each devices.

Sensors

Wiser Window/Door Sensor

Wiser Water Leakage Sensor

Wiser Motion Sensor

Wiser Temperature/Humidity Sensor

Lights

Iconic Connected Switch 10 AX / Iconic Connected Switch 2 AX

Wiser Micro Module Light Switch

Dimmers

Iconic Connected Dimmer

Wiser Micro Module Dimmer

Shutters

Wiser Micro Module Shades Control

Appliances

Iconic Connected Twin 10 A Socket

Safety

Wiser Smoke Alarm - Battery

Wiser Smoke Alarm 230 V

Fan Control

Iconic Fan Controller

Energy

PowerTag E

PowerTag C

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.