SUG_Wiser_Home_Australia_WHP-04

Editing a Schedule

In the Schedule details screen:

  • Tap (A) icon to change the name of the Schedule.

  • Select the Devices (B) the Schedule applies to.

  • Select the day (C) you want to add or edit events.

  • Tap (D) icon to edit an event.

  • Tap (E) icon to add an event to the selected day.

  • Tap (F) icon to copy a day or a Schedule.

Adding / Editing an event

  • Set the desired state (A).

    NOTE: The Device state will be different for individual Device types.
  • Set the time (B) of the event.

  • To save the event settings, tap Set.

  • To discard changes, tap Cancel.

  • To remove an event, tap Delete. (Not available when adding an event.)

NOTE: The available options and states are Device specific. Detailed information can be found in Device User Guide of the respective device. Refer to List of Wiser Devices for the links to Device user guide of each devices.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.