About Signal Strength
Signal Strength Indicator
There is four different levels of signal strength:
Good Signal (between 0 & -54dBm)
Cause of Poor Signal
Connectivity issues can be caused by various factors, such as:
-
Distance between the hub and devices - the signal becomes weaker as the devices move farther apart.
-
Physical Obstructions - doors, walls, furniture, household appliances, especially with metal surfaces, and other electronic devices can weaken the Zigbee® signal.
Troubleshooting
-
Place the hub into open space.
-
Make sure you check if all powered devices are switched on and working normally.
-
If possible, move the Wiser Hub closer to the device with signal issues.
-
Try to remove any physical obstructions between the Wiser Hub and the device with poor or no signal.
-
For battery-powered devices, check the battery level and replace the batteries if necessary.
Signal Extender
If you are still experiencing connectivity issues, we recommend adding lighting control devices such as a dimmer, switch, socket or blind control device etc. to your system. It has a built-in signal range extender that boosts the signal between your devices and the hub.
Help & Support
If you require further assistance, visit our Support Pages.
Help & Support:
For Australia, Visit: https://www.clipsal.com/wiser-home-customer-support