SUG_Wiser_Home_Australia_WHP-04

Limitations of the Wiser System

When commissioning a Wiser system, it is important to understand the system limits, such as the maximum number of supported devices.

System Limits

Maximum number of  

Devices total

128 (63 Zigbee devices + 1 Hub + 20 PowerTag + 1 Schneider Charge)

Rooms

16

Moments

20

Automations

10

Device Limits With Respect to Hub

Lights

Maximum overall

Maximum per Room

Lighting devices

32

32

Blinds

Maximum overall

Maximum per Room

Blind controller

32

32

Appliances

Maximum overall

Maximum per Room

Connected Socket

20

20

Fan Controller

32

32

Sensors

Maximum overall

Maximum per Room

Window + Door Sensor

10

10

Motion Sensor

10

10

Water Leakage Sensor

10

10

Temperature + Humidity Sensor

10

10

Infrascan Outdoor Motion Sensor 360

23

23

Safety and Security

Maximum overall

Maximum per Room

Smoke Alarm

16

16

Energy

Maximum overall

Maximum per Room

PowerTag

20

-

Schneider Charge

1

1

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.