SUG_Wiser_Home_Australia_WHP-04

Adding a Schedule

  1. On the Automation Screen (A), tap (B) icon.

  2. Enter a name in the text field (C).

  3. Select the Device type of the Schedule.

    IMPORTANT:
    • A Schedule can only be created for one Device type. If you want to switch a light at the same time as closing a blind, you will need to create two Schedules.

  4. Select the Devices to which the Schedule applies to.

    NOTE: All Devices of the selected Device type are available in the list.

  5. Tap Create (D).

  6. Tap (E) icon and set the details of the event.

    Find detailed information about adding events and editing Schedules in Chapter Editing a Schedule.

  7. Keep adding events until the Schedule is complete.

    NOTE: Changes to the Schedule will be saved immediately.
  8. When the Schedule is complete, tap Back (F) to save the schedule.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.