Safety devices
|
Wiser Smoke Alarm - Battery CLP599WSAL |
The Wiser Smoke Alarm - Battery uses a dual spectrum photoelectric sensor to detect smoke generated by fire. It also includes a temperature sensor that detects heat by rapid increase in temperature. When connected to the Wiser system, the device will send the notifications via the Wiser Home app. |
|
|
Smoke Alarm 240 V 755WSA |
The Smoke Alarm 240V uses a dual spectrum photoelectric sensor to detect smoke generated by fire. It also includes a backup battery that allows the device to work if the power supply is disconnected. When connected to the Wiser system, the device sends notifications to the user via the Wiser Home app.. |
|
|
Wiser Smoke Alarm 240V Square CLP599WSA |
The Wiser Smoke Alarm 240 V Square uses a dual spectrum photoelectric sensor to detect smoke generated by fire and a temperature sensor that detects heat caused by rapid increase in temperature. It also includes a backup battery that allows the device to work if the power supply is disconnected. When connected to the Wiser system, the device will send notifications via the Wiser Home app. |