SUG_Wiser_Home_Australia_WHP-04

Home Screen

Home Screen provides quick access to your favourite devices, lets you activate moments effortlessly, and offers personalized tips to help you maximize energy savings.

Home Screen:

A

Setting

Tap to navigate to the settings screen.

B

Favourite devices

You can add your most frequently used devices to the favourite section for quick access. Scroll horizontally to view all your favourite devices. Refer to Managing Favourites for information on how to add the devices to favourites.

NOTE:
  • If you have only one device installed in your home, this section will display it as Your device instead of Favourite devices.

  • If the device is currently following the schedule, it shows until when the current status will remain active based on the schedule. For example, here until 16:00 (H) means that device will stay On until 16.00.

C

Moments

You can view all the moments you have created for your home, allowing you to easily activate or deactivate them.

To rearrange the order of the moments:

  1. Tap Edit option.

  2. Drag and drop the moments to arrange them in your preferred order.

NOTE:  If you do not wish to see moments on your Home screen, go to  > Home Screen and disable the Show Moments toggle switch.
D

Tips and advice

Provides useful tips and advice to help you make the best use of your devices and optimize energy usage. Scroll horizontally or tap See all to view all the tips. Refer to Tips and Advice for more detailed information.

NOTE: If you do not wish to see Tips and advice on your Home screen, go to  > Home Screen and disable the Tips and advices toggle.

E

Energy

Tap to navigate to the Energy screen where you can monitor your energy consumption and production, view detailed history, and get information on energy savings.

F

Control

View/Control all the devices installed in your home, organized by the rooms to which they are assigned. Refer to Device Control for detailed information on how to control the devices.

NOTE: If you have only one device installed at your home, the Control tab will not be available.

G

Automation

Tap to navigate to the Automation screen, where you can set up Moments, Schedules, and Automations for your home. Please read the relevant Device User Guide of the device for more information. Refer to List of Wiser Devices for the links to Device user guide for each devices.

J

Banner

Provides important messages and notifications. These messages can include updates on device status, connectivity issues, and other relevant alerts to keep you informed about your home system.

Example:  In the current screen, the banner displays a message about a device being offline, along with information on how to improve signal strength. This helps you quickly identify and address any connectivity issues.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.