SUG_Wiser_Home_Australia_WHP-04

Blind controller

NOTE: If you are migrating from Wiser by SE to Wiser Home, make sure that all your devices are updated to the latest firmware version in Wiser by SE before migrating.

Wiser Micro Module Blind

CLP5015WBZ

The Wiser micro module blind is used to control one 240 V twin active blind/roller shutter motor equipped with an end position switch.

Instruction Sheet (PDF)

Device User Guide

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?