SUG_Wiser_Home_Australia_WHP-04

Enabling Wiser Home AI

The following is an example of enabling Wiser Home AI with Schneider Charge. installed.

To enable Wiser Home AI:

  1. On the Home screen, tap .

  2. Tap on the banner (A), then tap Try Wiser Home AI.

    NOTE: Wiser Home AI is free to use throughout 2025. In 2026, this feature will transition to a premium service with enhanced functionalities.

    TIP:
    • Tap (B) to understand more about the feature.

    • Tap (C) to read the terms and conditions.

  3. Tap Optimise your Home Profile > Continue to provide your daily schedule details and set up your profile.

  4. Set the time when you want your car to be charged:

    1. Tap (E), select a time period (F) and tap Set.

    2. Tap (G), select a time period (F) and tap Set.

  5. Tap Next.

  6. Enter the number of kilometers required to drive this car using the dial pad:

    1. Tap On week day

    2. Tap Over the entire weekend

  7. Tap Next.

  8. Tap Manage Wiser Home AI.

    You will be directed to Manage Wiser Home AI screen from the > Energy Management > Wiser Home AI to view the devices that are enabled.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?