SUG_Wiser_Home_Australia_WHP-04

Dimmers

NOTE:  If you are migrating from Wiser by SE to Wiser Home, make sure that all your devices are updated to the latest firmware version in Wiser by SE before migrating.

Wiser Micro Module Dimmer

CLP5010WDZ

The Wiser Micro Module Dimmer combines the advantages of smart dimmer functionality with ordinary mechanical push-button switches. It transforms a conventional switch into a connected device which can be controlled from the switch or through the Wiser Home app.

It can switch and dim the ohmic, inductive, or capacitive loads and it is also compatible with dimmable LEDs.

Instruction Sheet (PDF)

Device User Guide

Iconic Connected Dimmer

41EPBDWCLMZ-VW

The Iconic Connected Dimmer is a push-button device that can be used to switch and dim LED, ohmic or capacitive loads manually or remotely. It can detect the load automatically and provides thermal protection, overload-resistance and short-circuit protection.

Instruction Sheet (PDF)

Device User Guide

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?