SUG_Wiser_Home_Australia_WHP-04

Roles in the Wiser Home App

In the Wiser Home app, you can perform various tasks in the app, depending on the access level.

Function

Supported Features

Home owner

Professional Installer

Creating an account

Create an account by providing email address and setting up the password

Yes

No

Setting up the Wiser System

Adding and configuring the hub

and devices.

Yes

Yes

Manual Firmware Update

Updating the hub

firmware manually

No

Yes

Manage Rooms

Add or delete Rooms

Yes

Yes

Name or rename Rooms

Yes

Yes

Manage devices

Add or delete devices

Yes

Yes

Configure device feature setting and schedule

Yes

Yes

Change device icon, name and location

Yes

Yes

Control device

Yes

Yes

Receive device notifications and alarms

Yes

Yes

Manage Moments, Schedule and Automations

Create Moments, and Automations

Yes

Yes

Create or assign a Schedule.

Yes

Yes

Assign devices to Moments/Automations

Yes

Yes

Adjust device settings in Moments/ Automations

Yes

Yes

Set Trigger conditions in Moments/ Automations

Yes

Yes

Receive Moment/Automation trigger notifications

Yes

Yes

IMPORTANT:
  1. As a professional installer, the app offers for setting up a Wiser System and adding devices without having to be logged in.

  2. Any user can log in to the app, if the home owner provides the login credentials.

Professional Installer

This is a setup role by the Professional Installer. The main task of the Professional Installer is to set up the Wiser system.

To use the App as a Professional Installer:

  1. Tap Get started (A).

  2. Tap Professional Installer (B).

Home Owner

The Home Owner can create an account and set-up the Wiser system.

To use the App as a Home Owner:

  1. Tap Get started (A).

  2. Tap Home Owner (B) and create an account. Refer to Creating an Account for information on how to create an account.

    NOTE: After successfully creating your account using your email address and password, log in to the app and start using the Wiser system with your credentials.

Login to the App

  1. To login to the app, tap Login (A).

  2. Enter your credentials and tap Login (B).

    NOTE: You only have to log in to the app once. Each time you use the app again, you will be automatically logged in. You can log out of your account in the Account Settings.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?