SUG_Wiser_Home_Australia_WHP-04

Connected socket

NOTE:  If you are migrating from Wiser by SE to Wiser Home, make sure that all your devices are updated to the latest firmware version in Wiser by SE before migrating.

Iconic Connected Twin 10 A Socket

3025CSGZ

The Iconic Connected Socket Twin 10 A operates as a standard socket outlet “out-of-the-box”, with no configuration needed. It provides smart control of plug in appliances such as lamps, home theater equipment or hair straighteners.

Instruction Sheet (PDF)

Device User Guide

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?