DUG_2 Channel Relay Puck-00

Adding a new location

You can add a new location from the Settings menu.
  1. Tap Settings.
  2. Tap Location Settings.
  3. On the bottom right corner of the screen, tap +.
  4. Enter a new location name.
  5. Tap Add.
    NOTE: Alternatively, you can also create a new location from the Hamburger menu > + Add Location.
    TIP: If you want to switch to another location, navigate to the Hamburger menu and select the location you want to switch.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?