DUG_2 Channel Relay Puck-00

Editing an action

To edit an action:

  1. On the Actions page, tap Quick.
  2. On the top right corner of the screen, tap .
    The Edit Actions List page appears.
  3. From the Edit Actions List page, tap the action you want to edit.
    TIP: If you want the same action, tap the hand symbol, it will copy the same action and add it to the Edit Actions List.
  4. Tap each item (such as add, remove, rename, etc.) to update.
  5. Once all the edits are done, tap Update.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?