DUG_2 Channel Relay Puck-00

Resetting the device

You can reset the device to factory default manually.
Short-press the reset button 7 times (<10 s).
The LED rapidly blinks red after 10 s.

If the puck is inside the wall, you can toggle the external connected switch 14 times in 10 s to reset the device.

NOTE: After reset, the device is ready for pairing.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?