DUG_2 Channel Relay Puck-00

Changing the device location

You can change the device location using the Wiser app.

To change the device location:

  1. On the Devices page, tap Devices.
  2. Select the device for which you wish to change the location.
  3. On the top-right corner of the screen, tap Settings.
  4. Tap Information.
  5. Tap Change Room (A).
  6. Select the desired room from the list (B).
    NOTE: If your room name is not present in the list. You can create a new room using the + (C).
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?