DUG_2 Channel Relay Puck-00

LED indication

Pairing

User Action

LED Indication

Status

Press the reset button 2 times in 10 s.

Or

Toggle the external connected switch 4 times in 10 s.

Blinking red rapidly.

Pairing mode is active for 3 minutes. When pairing is completed, the LED will display a solid red.

Press the reset button 4 times in 10 s to change the Wi-Fi access point mode.

Or

Toggle the external connected switch 8 times in 10 s.

Blinking red rapidly.

The device is ready to connect with the new Wi-Fi network.

Resetting

User Action

LED Indication

Status

Press the reset button 7 times in 10 s.

Or

Toggle the external connected switch 14 times in 10 s.

LED blinks red.

The device is in reset mode. It is reset to the factory settings.

LED Indicator Mode

LED Indicator Mode

LED 1 Indication

LED 2 Indication

Always Off

Solid red

No LED

Load 1 On

Solid amber

No LED

Load 2 On

Solid red

Solid green

Device paired

Solid red

No LED

Device disconnected from the router after pairing

LED blinks red, once per 4 seconds

No LED

Reset state / Not paired / Not added

LED blinks red

No LED

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?