DUG_2 Channel Relay Puck-00

Removing the device

Using the Wiser app, you can remove a device from the device list.

To remove the device:

  1. On the Devices page, tap Devices.
  2. On the top right corner of the screen, tap .
    The Edit Device List page appears.
  3. Tap the remove button (A) which is next to the device name.
    The message pop-up appears.
  4. Tap Delete (B).
  5. Tap Delete Device (C) and then select Ok.
    NOTE: By removing the device, you will reset the device. If you still have a problem with the reset, then refer to Resetting the device.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?