DUG_2 Channel Relay Puck-00

Renaming the device

You can rename the device name using the Wiser app.

NOTE: You can also rename the other connected device using the below steps.

To rename the device:

  1. On the Devices page, tap Devices.
  2. Select the device for which you want to change the name.
  3. On the top-right corner of the screen, tap Settings (A).
  4. Tap Information.
  5. Enter the new name in the Name (B) field.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?