DUG_2 Channel Relay Puck-00

Using the device

The Control Panel allows you to switch on/ off and control various settings.
On the Devices page, tap Devices and select the device to access the control panel.

The control panel displays the following options:

  • Power Now (W): Displays the load value of the device (A).

  • Voltage (V): Displays the voltage of the device (B).

  • Current (A): Displays the flow of electric current of the device (C).

  • The current state of the device (F).

  • Settings (D)

  • Timeline (E)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?