DUG_2 Channel Relay Puck-00

Automate

Automate allows you to set the timing for when the device should be turned off and also set it to turn off when you are away.
  1. On the Devices page, tap Devices.
  2. Select the device.
  3. Tap Settings > Information > Automate.
  4. Tap the Auto-Off Timer (A) toggle button and set the time when the device should turn off.
  5. Tap the Away Mode (B) toggle button to switch off the device when you are away.
    NOTE: Use only one option at a time.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?