DUG_2 Channel Relay Puck-00

About this product

The 2-Channel Relay Puck (hereinafter referred to as puck) is a miniature micro module, which is remotely controlled and designed to operate in AC mains.
It enables remote control of two electrical appliances, each with a 5 A capacity. It provides app controlled switching of plug-in appliances with power monitoring feature using the Wiser app.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?