DUG_2 Channel Relay Puck-00

Pairing the device

Connect your mobile device with your home Wi-Fi network and use the Wiser app to access and control it.
To pair the device:
IMPORTANT: Before pairing the device, connect your mobile to the home Wi-Fi network.
  1. Open the Wiser app.
  2. On the Devices page, tap Devices.
  3. Tap + (A) to add a device.
    The Add Device page appears.
  4. The Add Device page includes the following tabs:
    • Preferred (B): This tab allows you to select a device directly from the preferred list.

    • All (C): This tab includes all available devices for you to select from.

    TIP: You can select a device from either tab based on your preference.
    • Select Preferred > Dual In-Wall Relay (Wiser).

    • Select All > Switches and Controls > Wi-Fi Switches and Controls > Dual In-Wall Relay (Wiser).

  5. Select any one of the following switch types based on your preference and tap Add (F):
    • ON/OFF Button (D)

    • Push Button (E)

  6. Press the reset button 2 times in 10 s.
    The LED indicator rapidly blinks red.
  7. Tap Next.
  8. Add the following Device Information:
    • Enter Device Name (G): Add the device name.

    • Assign Existing Room (H): Select an existing room.

    NOTE: If your room is not in the existing room, create a new one.
    • Add New Room (I): Create a new room.

  9. Tap Next.
    NOTE: To begin scanning for devices, make sure to enable Bluetooth permissions.
  10. Tap MAC ID (J).
    NOTE: If you are unable to find the device, tap Rescan (K).
  11. Tap Select Wi-Fi (L) and choose Wi-Fi network.
  12. Enter the Wi-Fi password in the password field.
    NOTE: After entering the password, the Connect (M) button will be enabled.
  13. Tap Connect (M).
    Now, you can see the newly added two devices on the Devices page.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?