DUG_2 Channel Relay Puck-00

Switching On/Off the device manually

When the puck is connected to a mechanical push button, the connected devices can be controlled manually by short pressing the push button.
NOTE: When the puck is installed inside the wall box, the status LED is not visible while using the puck.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?