5250CT9201

Cabinet Connector

The cabinet connector connects to the other devices in the same manner as a coupler.

Cabinet Connector
in. (mm)
Catalog Number Weight
lb. kg
6.00 (152) Duct

RWT06CC

0.9 0.4
10.00 (254) Duct

RWT10CC

1.3 0.6
18.00 (457) Duct

RWT18CC

2.4 1.1
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?