5250CT9201

Reducer Coupling

Reducers are occasionally required. The reducer is a coupling that allows the reduction to be made at any duct joint.

Reducer Coupling Type
in. (mm)
Catalog Number Weight
lb. kg
6.00–10.00 (152–254)

RWT06RC

1.5 0.7
10.00–18.00 (254–457)

RWTRC

2.1 0.9
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?