5250CT9201

Wire Retainer

Wire retainers are furnished for use at each duct joint. One additional retainer is furnished with each 5 ft (1.5 m) length to be field-installed in the center of the length at the cover plate joints. This is in order to close off any gaps between cover plates.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?