5250CT9201

Flush-to-Surface Adapter

Transitions from flush-to-surface mounted duct is made by the flush-to-surface adapter. The adapter mounts onto a flush-mounted cross. Flush-mounted straight lengths can be field modified to accept this adapter anywhere along a run.

Adapter Type
in. (mm)
Catalog Number Weight
lb. kg
10.00 (254)

RWT10FS

11.9 5.4
18.00 (457)

RWT18FS

16.4 7.4
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?