5250CT9201

Straight Lengths

Straight lengths are available in 5 (1.5 m) and 18 in. (457 mm) lengths.

Standard sizes are:

  • 6 x 3.5 in. (152 x 89 mm)

  • 10 x 3.5 in. (254 x 89 mm)

  • 18 x 3.5 in. (457 x 89 mm)

Covers are available for either flush- or surface-mounted installations.

  • 5 ft (1.5 m) duct lengths require two 30 in. (762 mm) covers

  • 18 in. (457 mm) duct lengths use one cover

Covers are field cut as required.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?