5250CT9201

Cross (Flush or Surface-Mounted)

Cross Type
in. (mm)
Catalog Number Weight
lb. kg
10.00 (254) with Flush Covers

RWT10XE

7.8 3.5
18.00 (457) with Flush Covers

RWT18XE

23.4 10.6
10.00 (254) with Surface Covers

RWT10XES

6.2 2.8
18.00 (457) with Surface Covers

RWT18XES

21.8 9.9
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?