5250CT9201

Elbow-Type Cabinet Connector

NOTE: All dimensions shown are for 10 in. (254 mm) wide duct with flush covers.

The elbow-type cabinet connector is used where surface mounted wall duct is run horizontally on a wall, above a cabinet requiring access from the top. Grommet material is supplied for cable protection around the field-cut openings.

Catalog Number Weight
lb. kg

RWT10SWEECC

12.0 5.4
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?