5250CT9201

End Cap

The end cap connects to the other devices in the same manner as a coupler. The end cap has a cover plate extension for use on flush mounted installations. This provides the system with the 1 in. (25 mm) cover plate overlap of the wall material. The cover plate extension is discarded on surface mounted installations.

End Cap
in. (mm)
Catalog Number Weight
lb. kg
6.00 (152) Duct

RWT06EC

1.0 0.4
10.00 (254) Duct

RWT10EC

1.3 0.6
18.00 (457) Duct

RWT18EC

1.8 0.8
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?