5250CT9201

Tunnel

The hole pattern in the coupler locates the straight partition to form a 3 in. (76 mm) wide compartment on either side of the straight length. The 3 in. (76 mm) compartment width is matched by tunnels for horizontal elbows, tees, and crosses. Tunnels are designed to form a 3 in. (76 mm) compartment as well. Hardware for mounting these devices into the fittings are furnished with the tunnels.

Tunnel Type
in. (mm)
Catalog Number Weight
lb. kg
10.00 (254)—Straight Through for Elbows

RWT10ST

2.9 1.3
18.00 (457)—Straight Through for Elbows

RWT18ST

3.8 1.7
10.00 (254)—90° Turn for Elbows

RWT10ET

3.2 1.4
18.00 (457)—90° Turn for Elbows

RWT18ET

5.1 2.3
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?