5250CT9201

Partition

Partitioning is often required in wall duct. A 5 ft (1.5 m) long straight partition is furnished for field installation. Holes are provided to mount the partition into the duct, forming a 3 in. (76 mm) wide compartment.

Partition
ft. (m)
Catalog Number Weight
lb. kg
5 (1.5) Partition

RWTP60

0.9 0.4
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?