AMI Post Installation Configuration
- Change the log file location, if required. By default the
log file will be placed in C:\Responder\Logs.
<file value="c:\responder\Logs\Miner.Responder.RxIF.AmiOutbound.log" />
- Change the MSMQ ComputerName to FQDN of the Responder Server.
Verify that the “ComputerName” is not populated, it should say “ComputerName”:
<wellknown type="Miner.Responder.Shared.IDataServices, Miner.Responder.Shared" url="msmq://FormatName:DIRECT=OS:{ComputerName}\private$\RxServer/DataServices.rem" />Set the “ComputerName” here:
<channel type="Miner.Responder.Shared.Channels.MSMQ.MSMQChannel, Miner.Responder.Shared" ComputerName="ComputerName" responseTimeout="00:06:00" />
- Application Configuration
Config Key
Config Description
Default Config Value
UseMsp
Flag to specify the head end is Multispeak or not.
TRUE
MspUrl
AMI Head end URL to submit the ping request.
https://<AMI Web Server Name>/multispeakv41/od
CimUrl
Url to the AMI CIM web service GetEndDeviceEvents endpoint
http://<AMI Web Server Name>/GetEndDeviceEvents
MspVersion
Version of the Multispeak supported by AMI Head end.
4
Ami.ProcessWaitInterval
Time between two subsequent processing cycles.
00:02:00
MeterPingMethod
Multispeak/CIM Meter Ping Methods.
http://www.multispeak.org/Version_4.1_Release/InitiateOutageDetectionEventRequest
BouncePingMethod
Bounce Ping Method, currently only used by CIM.
http://iec.ch/TC57/2011/EndDeviceEvents/CreatedEndDeviceEvents
InboundMspUrl
Multispeak OAServer URLs.
http://<AMI Web Server Name>/Miner.Responder.RxIF.Multispeak416/OAServer.asmx