Installation System Requirements

Operating Systems

The following operating system versions are required:
  • Windows Server 2012 and later

    • Windows Desktop 10 and later

    • Wiith IIS 7.5 or later

Microsoft .NET Framework Requirements

  • Version 4.6.1 and 3.5 of the Microsoft .NET Framework is required.

  • Microsoft .NET Framework requires client and extended installation

IIS Configuration Requirements

  • WCF Services for http should be enabled as a feature in the IIS server.

Oracle Pre-requisites

The following versions of Oracle Software and associated clients are supported:
  • Oracle 11g Client and later on Servers (32 bit)

  • Oracle ODAC 12c (32 bit)

Pre-requisite Software and Licensing

The following licensed software products levels are required:
  1. ESRI

    • ArcGIS 10.8.1

  2. Schneider Electric

    • ArcFM 10.8.1

    • Responder 10.8.1b

    • RxIF Module licenses

Testing Software

The following free tools are very useful for validating the configurations of RxIF and third party systems being integrated (AMI, SCADA, etc.). They are also invaluable for troubleshooting issues with communication between these systems.
  • Java Development Kit (JDK) (client)

  • Apache JMeter (client)

  • Wireshark (optional for troubleshooting) (Server)

  • Telerik Fiddler (Client)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?