SCADA Service
Installation Steps – SCADA Service Installation and Configuration
This is an optional module and is not required to run RxIF. However, RxIF Server is required before installing SCADA Service.
- Run the RxIF.ScadaService_####_Release installer.
In the Welcome dialog, click Next.TIP: The #### in the installer name represents the release number. For example, if you are installing 10.6.1b, the installer name is RxIF.ScadaService_1061b_Release, and the 10.8.1 installer name is RxIF.ScadaService_1081_Release.
- Type the Username and password of a domain or local user that will run the service. It must be a valid Responder user. Then click Next.
- Choose a database and click Next.
- Type the credentials for the database and click Next.
- Specify the MSMQ Server (eg., localhost, machinename@domain.com) and click Next.
- If ArcFM is installed, the same install location os used. Otherwise ensure that the location is set to C:\Program Files (x86)\Miner and Miner\ or use the Browse button to select it, and click Next.
- Start the installation by clicking on the Install button.