Database Configuration

  1. Open a command prompt and execute the install_cis.bat script.

    • For Oracle, the batch script is located in: C:\Program Files (x86)\Miner and Miner\Responder\Integration\CisSyncApplication\IntegrationScripts\Oracle
    • For SQL, the batch script is located in: C:\Program Files (x86)\Miner and Miner\Responder\Integration\CisSyncApplication\IntegrationScripts\MS-SQL

    This script requires the following files, which are in the same folder:

    1. CISConfiguration.sql

    2. CreateTables.sql

  2. Provide the Responder username, password, and database instance when prompted to do so, e.g.:

    • User name: responder (or any preconfigured user with DB admin rights)
    • Password@Instance: password@tnsname
  3. The batch script runs the SQL scripts to create the database structures listed below for the CisSync Application integration.

    • Adds the RXINT_CUSTOMERS_STAGE table.

    • Adds the Edit Customer Information role. This role has the Edit Customer Data task and is allowed to insert, update, and delete items from the RX_CUSTOMERS table.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?