Web Configuration for AMI Using MultiSpeak (optional module)
|
Config Key |
Config Description |
Config Value |
|---|---|---|
|
Ami.StaleEventThreshold |
Events received after this threshold compared to the system time are considered stale and not processed. |
02:00:00 |
|
Ami.MomentaryEventThreshold |
Time between PowerDown and PowerUp events that are within this threshold are considered momentary. |
00:01:00 |
|
Ami.EventMap |
Mapping of AMI Events defined in MultiSpeak and required in Responder.
NOTE: This setting appears only in MultiSpeak 3.0AB configuration.
It is not included in MultiSpeak 4.1.6.
|
Ami.DefaultEventMap |
|
Ami.CDEventMap |
Mapping of AMI Events defined in MultiSpeak for Remote Connect and Disconnect events and its required values in Responder. |
Ami.DefaultCDEventMap |
|
Ami.RequireDayLightAdjustment |
Set this flag if adjustment is required due to Daylight Saving Time. |
FALSE |
|
Ami.DayLightOffsetMins |
Configure the time adjustment required when Daylight Savings Time is in effect. |
60 |