SCADA Post Installation Configuration
C:\Program Files (x86)\Miner and Miner\Responder\Integration\Scada Outbound Service
or in the installed path if it was changed during installation.
- If required, Change the log file location. By default
the log file will be placed in C:\Responder\Logs.
<file value="C:\Responder\Logs\Miner.Responder.RxIF.ScadaOutboundService.log" />
- Change the MSMQ ComputerName to the FQDN of the Responder
Message Router Server.
Verify that the “ComputerName” is not populated, it should say “ComputerName”:
<wellknown type="Miner.Responder.Shared.IDataServices, Miner.Responder.Shared" url="msmq://FormatName:DIRECT=OS:{ComputerName}\private$\RxServer/DataServices.rem" />Set the “ComputerName” here:
<channel type="Miner.Responder.Shared.Channels.MSMQ.MSMQChannel, Miner.Responder.Shared" ComputerName="ComputerName" responseTimeout="00:02:00" />
- Application Configuration
Config Key
Config Description
Default Config Value
ScadaInterface.ServiceName
Configuration for the Outbound service to Identify the Scada Service Specification
MultiSpeak30ab
ProcessWaitInterval
Time between two subsequent processing cycles
00:00:15
MultiSpeak.ApplicationName
Standard detail for the Outbound message header.
Responder OMS
MultiSpeak.ApplicationVersion
Standard detail for the Outbound message header.
10.6.1a
MultiSpeak.Company
Standard detail for the Outbound message header.
Schneider Electric
MultiSpeak.UserID
Standard detail for the Outbound message header.
sample
MultiSpeak.Password
Standard detail for the Outbound message header.
sample
CallRemarks
Remarks on Calls created by IVR.
Remarks on Calls created by IVR.
IvrCallRecordId
Custom field added to the RX_CALLS table to maintain the call ID for a call record in the IVR system. Used when callbacks or close calls requests are submitted once the incident is restored.
RXINT_CALL_RECORD_ID
StaleEventThreshold
EVENTTIME timestamp in HTTP endpoint data received over this threshold compared to system time are not processed and are errored out back to the source system.
02:00
MomentaryEventThreshold
Time between PowerDown and PowerUp events that are within this threshold are considered momentary. Note: if the RECIEVETIME of the event at the HTTP endpoint is greater than the PowerUp EVENTTIME, then the event will not be treated as momentary.
00:00:30
FilterDuplicates
Multiple incidents will not be created when SCADA events are created for the same device.
TRUE
Scada.EventMap
The optional configuration available to map the SCADA system status to the Responder device status.
Scada.EventMap
ScadaIncidentRemarks
Remarks on Incidents created because of SCADA device operation
Created by SCADA.
ScadaClassModelName
Class model name to be assigned to identify the SCADA device in the geodatabase.
SCADAFEATURECLASS
ScadaFieldModelName
Field model name to identify the Scada Device using the Field assigned this model name.
SCADADEVICEID
- Change the MockServices URL to point to your SCADA system’s
web services. The underlined portion in the code below needs to be
changed in both places. The new endpoint address will look similar
to http://123.456.78.9/msscada/SCADA.
<client> <!-- MultiSpeak 416 Scada Service config --> <endpoint address="http://localhost/Miner.Responder.RxIF.MockServices/ScadaServer416.asmx" binding="basicHttpBinding" bindingConfiguration="SCADA_ServerSoap" contract="MultiSpeak416ScadaService.SCADA_ServerSoap" name="ScadaServer416Soap"/> <!-- MultiSpeak 30ab Scada Service config --> <endpoint address="http://localhost/Miner.Responder.RxIF.MockServices/ScadaServer30ab.asmx" binding="basicHttpBinding" bindingConfiguration="SCADA_ServerSoap" contract="MultiSpeak30abScadaService.SCADA_ServerSoap" name="ScadaServer30abSoap"/> </client>
- If you are using MultiSpeak3.0ab, you’ll need to
change the commenting on a couple items. You will need to comment
out the line for MultiSpeak4.1.6, and uncomment the line for MultiSpeak3.0ab,
so the two lines looks as follows:
<add key="ScadaInterface.ServiceName" value="MultiSpeak30ab"/> <!--<add key="ScadaInterface.ServiceName" value="MultiSpeak416"/>-->