Web Configuration for AMI Using CIM (optional module)
|
Config Key |
Config Description |
Config Value |
|---|---|---|
|
Ami.StaleEventThreshold |
Events received after this threshold compared to the system time are considered stale and not processed. |
02:00:00 |
|
Ami.MomentaryEventThreshold |
Time between PowerDown and PowerUp events that are within this threshold are considered momentary. |
00:01:00 |
|
Ami.EventMap |
Mapping of AMI Events defined in CIM and required in Responder. |
Ami.DefaultEventMap |
|
Ami.PingResponseMap |
Mapping of AMI Events defined in CIM and required in Responder. |
Ami.DefaultPingResponseMap |