CIS Sync Application

  1. Run RxIF.CisSyncApplication_####_Release.msi installer. In the Welcome dialog, click Next.
    TIP: The #### in the installer name represents the release number. For example, if you are installing 10.6.1b, the installer name is RxIF.CisSyncApplication_1061b_Release.msi, and the 10.8.1 installer name is RxIF.CisSyncApplication_1081_Release.msi.
  2. If ArcFM is installed, the same install location will be used. Otherwise ensure that the location is set to C:\Program Files (x86)\Miner and Miner\ or use the Browse button to select it, and click Next.
  3. Start the installation by clicking on the Install Button.
The installation will complete and the files will be deployed to C:\Program Files (x86)\Miner and Miner\Responder\Integration\CisSyncApplication.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?