SCADA Database Configuration
-
Open a command prompt and the execute install_Scada.bat script.
-
For Oracle, the batch script is located in:
C:\Program Files (x86)\Miner and Miner\Responder\Integration\Scada Service\IntegrationScripts\Oracle
-
For MS-SQL, the batch script is located in:
C:\Program Files (x86)\Miner and Miner\Responder\Integration\Scada Service\IntegrationScripts\MS-SQL.
This script requires the following files, which should be in the same folder:
-
01_RxScadaCustomTables.sql
-
-
Provide the Responder Username, password, and database instance when prompted to do so. For example:
User name: responder (or any preconfigured user with DB admin rights)
Password@Instance: password@tnsname
The batch script runs the SQL scripts to create the necessary database structures for the SCADA integration as listed below.
-
Adds the following tables:
-
RXINT_SCADA_EVENT
-
RXINT_SCADA_EVENT_PROCESS
-
RXINT_PROCESS_LOGS
-
-