Configure Display Persist Time for Ping Requests
When a user performs a ping request, a record of that request and its results is created in Responder Explorer > Ping Requests tab.
Users are not able to manually remove ping request records from this tab. Instead, you configure at a system level how long these ping request records are viewable in the Ping Requests display.
To set the persist time for ping request records, follow these steps:
- Navigate to the folder C:\Program Files (x86)\Miner and Miner\Responder\Integration\Ami Outbound Service
- Open the Miner.Responder.RxIF.AmiOutboundService XML configuration file in a text editor such as Notepad ++.
- Locate the appSetting “Ami.PersistMeterPingDuration”TIP: The easiest way to locate the proper setting is to search for PersistMeterPing.
- Set the duration value. The time format of the value is
hr:min:sec. In the following example, it is set to 8 hours. Ping requests
older than this value are removed when the TableMaintenanceProcessor
runs (the TableMaintenanceProcessor interval is also configured in
the same XML configuration file).
<appSettings> <add key="Ami.PersistMeterPingDuration" value="08:00:00" /> </appSettings>
- Restart the RxIF AMI Outbound Service to enact your change for your users.