IVR Service Configuration
Update the application configuration file Miner.Responder.RxIF.IvrOutboundService.exe.config located in the folder C:\Program Files (x86)\Miner and Miner\Responder\Integration\Ivr Outbound Service or the installed path, if it was changed during installation.
-
In the Miner.Responder.RxIF.Rx section, change the MSMQ ComputerName to the FQDN of the Responder Server.
Change the computer name to the computer where Rx Data services are running with out curly braces.
<wellknown type="Miner.Responder.Shared.IDataServices, Miner.Responder.Shared" url="msmq://FormatName:DIRECT=OS:{ComputerName}\private$\RxServer/DataServices.rem"/> </client> <channels>Change the computer name to the computer where MSMQ services are running.
<channel type="Miner.Responder.Shared.Channels.MSMQ.MSMQChannel, Miner.Responder.Shared" ComputerName="ComputerName"/>
-
If required, change the log file location. By default the log file will be placed in C:\Responder\Logs.
<file value="C:\Responder\Logs\Miner.Responder.RxIF.IvrOutbound.log"></file>
-
Application Configuration
|
Config Key |
Config Description |
Default Config Value |
|---|---|---|
|
UseCallsInsteadOfCallbacks |
When true, this generates a callback for all callers even if a callback is not requested. |
TRUE |
|
CloseCallbacks |
Determines if Callback is removed from the Callbacks tab after processing. |
TRUE |
|
IncidentFields |
ID,TIME_RESTORED |
|
|
MspUrl |
End Point URL for submitting IVR transactions |
http://domainname/service |
|
Ivr.ProcessWaitInterval |
Time between two subsequent processing cycles. |
00:02:00 |