Web Configuration for IVR with MultiSpeak 4
|
Config Key |
Config Description |
Config Value |
|---|---|---|
|
IVREnabled |
Determines if IVR is enabled. |
True |
|
IvrLocationCallRemarks |
The value of the remark for location calls created by IVR when the account number and phone number cannot be found for the caller. |
Location Call By IVR, Telephone Number:, Call Back:, Caller ID:, Comments:
|
|
IvrAppendCommentsToCallRemarks |
Determines whether to append the comments in outageDetection.Event.comments to the value of IvrCallRemarks when setting the Call Remarks. |
|
|
IvrSetCallOrigination |
Determines the value for the call’s Origination. |
|
|
IvrInvalidCallTroubleCodes |
If a trouble code defined in the Int_TroubleCode domain and specified in this field is returned by IVR, do not create the call. |
Format is InvalidCode1,InvalidCode2 |
|
IvrAlwaysPopulateCallBackNumber |
Determines whether the RX_CUSTOMER.CALLBACK_NUMBER field is populated. |
|
|
IvrCustomFields |
This setting is used to set a custom field in the RX_CALLS table. This field must already exist in the table. |
Format is IVRKey1,CALLS_FIELD1;IVRKey2,CALLS_FIELD2 IVRKey[#] is the message field to update and CALLS_FIELD[#] is the RX_CALLS field to update. For example, setting this to "VoiceMailFlag,VOICE_MAIL" would retrieve the VoiceMailFlag value from the input message and update the RX_CALLS.VOICE_MAIL field. |
|
IvrCustomFieldsDateTimeFormat |
This setting allows for the format specification for any custom field whose type was set to “dateTime.” |
yyyy'-'MM'-'dd'T'HH':'mm':'ss.fffK |
|
IvrPhoneSearchWithNoAccountNumber |
If no account number exists for a customer, search for the phone number, and if found, create a call. |
|
|
IvrCustomSearchFields |
If IvrPhoneSearchWithNoAccountNumber is true and no account or phone number exists for the customer, search on the fields specified in this setting. |
Format is IVRKey1,SEARCH_FIELD1;IVRKey2,SEARCH_FIELD2 IVRKey[#] is the message field to search on and SEARCH_FIELD[#] is the RX_CUSTOMERS field to search on. For example, "MessageLastName,LASTNAME;MessageFirstName,FIRSTNAME" would compare the MessageLastName value from the input message against the RX_CUSTOMERS.LASTNAME and the MessageFirstName value from the input message against the RX_CUSTOMERS.FIRSTNAME |
|
IvrSearchCustomFieldsUsingAnd |
Determines whether to use “and” or “or” for multiple search terms. |
|
|
IvrSubmitLocationCalls |
Create a location call if no phone number or account number is found. |
|
|
IvrCrewOnSiteCodes |
This setting defines the codes that denote that a crew is onsite. The codes can be configured in the CREW_ASSIGNMENT_STATUS domain in DatabaseSchemaConfig. |
3,4 |
|
IvrCrewDispatchedCodes |
This setting defines the codes that denote that a crew has been dispatched. The codes can be configured in the CREW_ASSIGNMENT_STATUS domain in DatabaseSchemaConfig. |
2,3,4 |