Construct the Fiber Optic Cable Favorite
- In ArcMap, apply a Stored Display that includes your fiber features.
- Start Editing.
- In the Table of Contents, click the Features pane.
- Navigate to the folder that will contain your fiber favorites.
- If you do not have a favorite folder yet, right-click a desired location and choose Create Favorite Category, name it, then click OK.
- Right-click the favorite folder and choose Create Favorite.
- On the Select a Target dialog, choose Fiber Cable, then click OK. The Create Favorite dialog opens.
- For Description, type a descriptive name such as 144 Count Distribution
- Fill out as many common fields as you can for the cable.TIP:
-
This is a favorite that will be used over and over again. You do not want to enter information such as Name, Date Installed, Installed by, or any other unique identifiers, as these vary from cable to cable. Instead, focus on attributes that are common for these types of cables. For example, if your company always uses the same Manufacturer, Contractor, Enclosure Type, etc., fill those fields in as defaults for the fiber users.
-
When creating a favorite, there are many attribute fields to populate. When inside the Create Favorite dialog, press the Up and Down keys to move through the fields, and press the Enter key to activate the field.
IMPORTANT: You might be wondering if you need to type in the various model names. The answer is no. These automatically populate when you bring the favorite into the ArcFM Attribute Editor > Targets tab, which occurs before you sketch the favorite on the map. In other words, given the auto-updaters assigned to these fields, the application handles the model names fields for you. -
- Click Apply.
- Expand the favorite to see its child relationships.
- Right-click F_BUFFERTUBE and choose Add Related Object.IMPORTANT: In the standard data model, Buffer Tubes only have unique attributes such as color, number, and name. Thus, for now leave the buffer tube un-attributed. When all tubes are in place, you return and add the unique attributes.
- Expand BufferTube to see its relationships.
- Right-click F_FIBER and choose Add Related Object.
- Fill out as many common fields as you can for the fiber.IMPORTANT: As a friendly reminder, stick to common attributes for now. After copying and pasting, you return to each fiber and add unique attributes such as number and color. Because you will ultimately paste this fiber many times, double-check the attributes for accuracy.
- Click Apply.
- Right-click Strand and choose Copy.
- Right-click F_FIBER and choose Paste (or press Ctrl + V).
- Repeat 10 more times so that you have 12 Strands total.
- This has been a good amount of work so far, and it would
be wise to save at this point:
- In the Create Favorite dialog, click Create, then click Close.
- On the Editor toolbar, click Editor > Save Edits.
- When prompted to save changes to feature favorites, click Yes.
- To continue editing the favorite, in the Table of Contents > Features pane, right-click the Cables and choose Edit Favorite.
- Expand the relationships again until you see all the Strands.
- Click the top-most Strand so that it is highlighted in blue.
- For Description, type BlueIMPORTANT: These steps follow the standard color-coding pattern used by the Fiber Optic Association (FOA)
- Add the Color and Name attributes for the Blue fiber.
- Color: Blue
- Name: BL
IMPORTANT: You might be wondering about the Num field at this point. Eventually, this is populated, but because each tube has a Blue fiber, do not populate this field just yet. After copying and pasting it throughout the tubes, you return and provide the unique number. Otherwise you would be copying the wrong number for all subsequent tubes.
- Click Apply.
- Click the second Strand so that it is highlighted.
- For Description, type Orange
- Add the Color and Name attributes for the Orange fiber
- Color: Orange
- Name: OR
- Click Apply.
- Repeat this process until all Strands have a Description, Color, and Name, all corresponding to your color-coding system (again, these steps use the standard system as approved by FOA).
- Save your favorite, and then return to editing the favorite.
- You currently have a single tube with 12 fibers, all with
common attributes. To build out the remaining tubes:
- Right-click the BufferTube and choose Copy.
- Right-click the F_BUFFERTUBE relationship and choose Paste (or press Ctrl + V).
- Repeat 10 more times so that you have 12 BufferTubes total.
- Click Apply.
- Save the favorite.
- Return to editing the favorite.
- It is time to make the buffer tubes and fibers unique. For buffer tubes, this means adding a Description, Position, Num, Color, and Name. For fibers, the only remaining attribute is the Num.
- Click on the top-most BufferTube and add the unique attributes:
- Description: Blue
- Position: 1
- Num: 1
- Color: Blue
- Name: BL
- Click Apply.
- Under the Blue buffer tube, expand F_FIBER to see the individual fibers.
- Proceeding through each fiber, add the Num attribute, starting with the number 1 for the Blue fiber, 2 for the Orange fiber, 3 for the Green fiber, etc., ending with the number 12 for the Aqua fiber.
- Click Apply.
- Use the following table as a guide to populate all the
BufferTube attributes and the fiber numbers.TIP:
-
These are a lot of identifying numbers. Remember each tube’s fibers should end at an increment of 12.
-
It is recommended to save after completing each tube, at the very least.
BufferTube Description
BufferTube Position
BufferTube Number
BufferTube Color
BufferTube Name
Fiber Color
Fiber Num
Blue
1
1
Blue
BL
Blue
1
Orange
2
Green
3
Brown
4
Slate
5
White
6
Red
7
Black
8
Yellow
9
Violet
10
Rose
11
Aqua
12
Orange
2
2
Orange
OR
Blue
13
Orange
14
Green
15
Brown
16
Slate
17
White
18
Red
19
Black
20
Yellow
21
Violet
22
Rose
23
Aqua
24
Green
3
3
Green
GR
Blue
25
Orange
26
Green
27
Brown
28
Slate
29
White
30
Red
31
Black
32
Yellow
33
Violet
34
Rose
35
Aqua
36
Brown
4
4
Brown
BR
Blue
37
Orange
38
Green
39
Brown
40
Slate
41
White
42
Red
43
Black
44
Yellow
45
Violet
46
Rose
47
Aqua
48
Slate
5
5
Slate
SL
Blue
49
Orange
50
Green
51
Brown
52
Slate
53
White
54
Red
55
Black
56
Yellow
57
Violet
58
Rose
59
Aqua
60
White
6
6
White
WH
Blue
61
Orange
62
Green
63
Brown
64
Slate
65
White
66
Red
67
Black
68
Yellow
69
Violet
70
Rose
71
Aqua
72
Red
7
7
Red
RD
Blue
73
Orange
74
Green
75
Brown
76
Slate
77
White
78
Red
79
Black
80
Yellow
81
Violet
82
Rose
83
Aqua
84
Black
8
8
Black
BK
Blue
85
Orange
86
Green
87
Brown
88
Slate
89
White
90
Red
91
Black
92
Yellow
93
Violet
94
Rose
95
Aqua
96
Yellow
9
9
Yellow
YL
Blue
97
Orange
98
Green
99
Brown
100
Slate
101
White
102
Red
103
Black
104
Yellow
105
Violet
106
Rose
107
Aqua
108
Violet
10
10
Violet
VL
Blue
109
Orange
110
Green
111
Brown
112
Slate
113
White
114
Red
115
Black
116
Yellow
117
Violet
118
Rose
119
Aqua
120
Rose
11
11
Rose
RS
Blue
121
Orange
122
Green
123
Brown
124
Slate
125
White
126
Red
127
Black
128
Yellow
129
Violet
130
Rose
131
Aqua
132
Aqua
12
12
Aqua
AQ
Blue
133
Orange
134
Green
135
Brown
136
Slate
137
White
138
Red
139
Black
140
Yellow
141
Violet
142
Rose
143
Aqua
144
-
- Save the favorite.