Fiber Mode

TIP:
  • This domain is not required but modetype functionality and counting ability in Fiber Manager need a field with these particular values.

  • Coded values other than the ones below are not supported.

  • These values don’t have to be stored in a domain, but doing so means less typing for users.

Properties:

  • Field Type: Text

  • Domain Type: Coded Values

  • Split Policy: Duplicate

  • Merge Policy: Default Value

Coded Values:

Code

Description

Multimode

Multimode

Singlemode

Singlemode

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?